2/8/2017 2:32 PM | |
Joined: 9/8/2016 Last visit: 6/29/2024 Posts: 198 Rating:
|
Hi, I've (again) couple of questions about WinCC. Right now i stuck with AlarmControl. I think the answers must be simple and with your help a can go forward. Acording to the attached element (in attachement you can find zip file with png pictures for faster understand things about i want to ask). Picture 1a/1b/1c - from WinCC 6.2. In 1a there is showed specific alarm setting from selected Class/Type Alarm. And there is only "will be archived" optiom marked. So: Question 1 - it means, that specific alarm will be only archived and don't need any acknowlegment? It will be showed on WinCCAlarmControl and automaticly dissapear when condition - go to false. Picture 1b is about setting for class. It has marked only "Separate Ack Key". Question 2 - What does it means? Picture 1c is a result - alarm control showed in runtime. I trigger alarm manually and Question 3 - the button for acknowlegment is always greyd (single or group). Is that situtaion is ok? Picture 2 is a setting from WinCC 7.4 from the same project (migrated, of course). It has only "Acknowlegment key" optiom marked but alarms are wok the same like above. The acknowledgment buttons are always greyd on runtime. And alarms dissapear when conditions go to false. Question 4 - in this case what do that option? Picture 3. I build alarm on brand new project and i have grayed option to change date format. Acording to manual we can choose where to change options for alarms. The 1st one is from WinCCAlarmControl or from AlarmLogging Explorer. I choose the second one and i have marked in WinCCAlarmControl option "Apply project settings". So everything - date format, column width (amount of char) i should able to change from AlarmLogging Explorer. But i can't. Anybody know why? Any advise will be very helpfull AttachmentWinCC_Alarm_Questions.zip (112 Downloads) |
Follow us on