3/4/2017 4:37 PM | |
Joined: 9/2/2012 Last visit: 8/15/2024 Posts: 711 Rating: (30) |
Hi, The stop mode issue is resolved. It was problem with Rse settings. Other questions ? |
|
|
3/6/2017 12:04 PM | |
Joined: 9/2/2012 Last visit: 8/15/2024 Posts: 711 Rating: (30) |
update... Tested FB126, RSE with step7 + wincc flexible combination. Working ok. Migrated flexible project to TIA (wincc comfort v13 sp1 upd8), added PLC via device proxi and tested, working ok with 1 problem. FB126 functionality for the node overview is working ok(tested for profinet) But with RSE, error is generating, but not showing any error text. If i check the controller message, alarm entries are there, but not showing any text. Tried migration many time, but same result. Compile also showing the warning about alarm text.. pfa AttachmentRSE.zip (206 Downloads) |
|
|
Follow us on