3/9/2017 10:25 AM | |
Posts: 6 Rating: (2) |
Hello, Linked to these problems it looks like PLCSIM Communication 1200/1500 does not exist in PLCSIMV14, but may be it is necessery to have it. I use to do simulations on virtual machine for PLC and HMI. Everything was working well with plcsim V13. But now my virtual machine (Win7 x64) only have TIA portal pro V14 with PLcsim V14 WinnCC confort/advanced V14, and it is not possible to select PLCSIM 1200 1500 with the settings of the PG adapter. Whats happen: When I simulate PLC there is no problem, but when I simulate a HMI it is definitly not possible to get a connection with the simulated CPU. So I will try to install PLCSIM V13 to get the channel PLCSIM 1200/1500 communication and look if it is fuctionning again. If you have already try it let me know best regards Jean-Michel ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 3/9/2017 2:28:09 PMNew subject after splitting |
|
3/9/2017 10:27 AM | |
Joined: 5/12/2006 Last visit: 5/2/2024 Posts: 22243 Rating: (2981)
|
Hello, with PLCSIM V14 you must use the "PLCSIM" insteed of "PLCSIM S7-1200 / S7-1500".
Christoph |
3/9/2017 10:55 AM | |
Joined: 5/12/2006 Last visit: 5/2/2024 Posts: 22243 Rating: (2981)
|
Hello, have you also checked that the devices in the project have the correct versions? https://support.industry.siemens.com/cs/ww/en/view/109742764 Regards Christoph |
Last edited by: ChristophD at: 3/9/2017 10:56:10 AM |
|
3/9/2017 11:13 AM | |
Posts: 6 Rating: (2) |
Yes Christophe you are rigth, I have just find it and it works. Thanks Best regards Jean-Michel |
Follow us on