Industry Online Support
Technical Forum
5/13/2008 9:12 AM | |
Posts: 86 Rating: (1) |
Thank you Billwest I have already usedDynamic Dialog to monitor tag status and change colors. This dynamic dialog is used for a specific tag in one connection. but i want to monitor the connection tags without external tags creation. I found an command in graphic designer: Dynamic wizard>>create a redundant connection this command creates a connection specific tags in the related connection. but there is a big problem: the created tags have the same address with the last external tag created in the whole project. I couldn`t solve this problem. AttachmentConnection tags.zip (100 Downloads) |
5/13/2008 10:40 AM | |
Posts: 1776 Rating: (95)
|
Hi, use the lifebeat monitoring -- see the online description |
Follow us on