3/15/2017 5:59 AM | |
Posts: 1 Rating:
|
Hi All, I am seeing a tag logging issue that has me stumped. I have multiple tags in Tag Logging that are configured effectively the same, but are behaving very differently.The incorrectly behaving tags should only log a value once day or so, but are instead logging a value every second! The strangest thing is that tags that are configured the same are behaving differently. The tags in question have the following settings: These tags also very rarely change value, so I would expect them to be logged one a day (because of the segment set-up). While some tags behave as expected, several do not, several are recording a value every second. Refer to the attached spreadsheet for an export of the tag logging configuration. I have changed some names to keep the info anonymous. 1. Why are tags that are configured the same behaving so differently? Has anyone experienced anything similar? Would greatly appreciate your help.
Johanne AttachmentTag_0603_vs_Tag_0150.xlsx (48 Downloads) |
Follow us on