7/29/2014 5:02 AM | |
Posts: 3 Rating: (0) |
Hello, I'm kinda of in a pinch, a customer of mine has an S7-300 PLC and has sent me the program (I program across a few platforms but this is not one we see often). Theres a bit addressing error, I'm assuming a typo but I cant open the file to see where the mistake is. I've downloaded Step 7 lite but it wont open the .S7P files, I know it can be opened in Step 7 Pro, then I could export the complete program as an *.awl file. and symbol table as an *.sdf file. Would there be anyone willing to do this for me? I dont need to modifiy the program I just need to see where a totalizer is located and change it in the quick panel software that I do posess, its preventing this customer from coming back online. Thanks in advance, Ryan AttachmentARE_RO_A_PLC_101117.zip (156 Downloads) |
7/29/2014 7:45 AM | |
Joined: 4/22/2010 Last visit: 2/15/2024 Posts: 5697 Rating: (713)
|
Hello, Attached you find the files. Hope it works for you now. Regards, Marcjan Attachmentconverted_files.zip (151 Downloads) |
Problem solved? |
|
7/29/2014 8:37 AM | |
Joined: 4/22/2010 Last visit: 2/15/2024 Posts: 5697 Rating: (713)
|
Hello, The adress is written to in FC7 NW9 (ADD instruction) Regards, Marcjan AttachmentFC7.pdf (97 Downloads) |
Problem solved? |
|
3/24/2017 1:58 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4774 Rating: (123) |
New question published by alexpaper is split to a separate thread with the subject How you exported Step 7 source file to .awl. Best regards |
Follow us on