3/25/2017 6:24 AM | |
Joined: 9/9/2015 Last visit: 7/16/2024 Posts: 727 Rating: (273) |
I have another easier way of doing this. You may use the SFC Position Text (POSINO) function to achieve what you want. However, you may need to modify the SFC Type. Here attached with a picture. Basically, I just create POSINO using SFC type characteristics, and branch out multiple routes. When you selected your destination, the desired position text will be display. The POSINO of SFC type has the attribute of S7_m_c. you can use text list in wincc to display your text (simpler method), or use back the SFC visualization standard faceplate. the position text will be displayed there. This is just a suggestion. Hope it helps~ |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
Follow us on