3/27/2017 2:06 PM | |
Joined: 12/18/2014 Last visit: 4/28/2024 Posts: 32898 Rating: (4067)
|
You have unfortunately in the LOGO! no way to make comparisons of time and / or date directly. If you want to trigger a specific event at a specific time, this only takes place via the weekly timer and / or the year timer. You can then change the parameters of the date and time via the TDE when you call the corresponding parameters in a message text. AttachmentWeekly_timer_0BA8.Standard.zip (193 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on