3/26/2017 10:18 AM | |
Joined: 12/22/2006 Last visit: 1/25/2022 Posts: 1742 Rating: (309) |
Hello, To load a FW 2.0, you would need the hardware 516-3AN01 And you cannot upgrade a 516-3NA00 hardware to 516-3NA01 by yourself. |
Last edited by: jklm at: 3/26/2017 10:21:45 AMBest regards |
|
3/28/2017 3:43 PM | |
Joined: 12/13/2011 Last visit: 4/19/2023 Posts: 123 Rating: (14) |
Thank you for the response. My issue is I need the following feature in the SIPLUS version of the 1516 CPU: New features with firmware V2.0 CPU:
Is there any time line for a 1516 6AG1 516-3AN01 firmware version 2.0? Regards, masmith1553 |
3/28/2017 3:57 PM | |
Joined: 5/12/2006 Last visit: 10/8/2024 Posts: 22399 Rating: (3017) |
Hello, for the SIPLUS PLC you use the same FW Files like the non SIPLUS. So you can easy download the FW from here:
|
3/28/2017 8:24 PM | |
Joined: 12/13/2011 Last visit: 4/19/2023 Posts: 123 Rating: (14) |
Christoph, Where can I find the support package for the SIPLUS 1516 3AN01 CPU? I cannot see this CPU in my hardware table. Regards, masmith1553 |
Follow us on