10/8/2013 10:11 AM | |
Joined: 4/29/2010 Last visit: 7/15/2024 Posts: 1557 Rating:
|
Hello Nikzitronik, please take a look at the communication manual of WinCC flexible: SIMATIC HMI WinCC flexible 2008 Communication Part 2 The ABB AC500 PLC isn´t aviable in flexible (see chapter ABB in the manual). With best regards |
10/9/2013 12:02 PM | |
Posts: 150 Rating:
|
Dear All, I managed to find a way to connect the AC500 with WinCC Flexible. Attached you will find the programm for AC500, WinCC Flexible, part of the manual for the AC500 manual and a Control Builder Screenshot. The way to do this is the following: AC500 is capable of communicating via Modbus TCP/IP. So the ethernet port needs to be parametrized for Modbus TCP/IP. It is important to set the "server connections" to something greater than 1 (see attached screenshot). The default setting is zero and if it is left to zero then no communication can be initiated. In the Flexible side, Configure a Modicon Modbus TCP/IP connection. Care must be taken to do the addressing correct (see atteched extract from AC500 manual). In the AC500 MW are splitted in segments depending on the CPU memory capacity i.e. %MW0.100, %MW1.100 etc. In the tags the address of %MW0.100 is %MW100. For bit tags bits need to be extracted from the MW. So as per the manual the byte order is motorola and the byte addresses are 2n and 2n+1 of MWn. For example: %MW100.0 in WinCC Flex is %MX0.201.0 %MW100.8 in WinCC Flex is %MX0.200.0 Regards Nik AttachmentAC500.zip (575 Downloads) |
Last edited by: Nikzitronik at: 10/9/2013 12:03 PM |
|
This contribution was helpful to
5 thankful Users |
11/30/2014 9:33 AM | |
Posts: 2 Rating:
|
Nikzitronik Do you see advantages of using WinCC Flex with ac500 in comparing of using WinCC Flex with s7? Programming, commissioning of ac500? Thnx
|
12/1/2014 4:46 PM | |
Posts: 2 Rating:
|
Nikzitronik thanks for reply. Why not web visualisation?
|
4/5/2017 3:02 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4770 Rating:
|
New question published by Rajnish% is split to a separate thread with the subject Wincc V7 communication with ABB AC500. Best regards |
Follow us on