Industry Online Support
Technical Forum
1/31/2008 8:27 AM | |
Posts: 76 Rating: (16) |
dear everybody , I've a s7-300 plc when i'm trying to down load program to my cpu after completing the download it goes into stop mode and lf & sf leds flash rapidly . when i downloaded it on another plc of same type and cpu it works properly. here is the archived edition of my prog. . It was for communication with PA devices . every thing are included in the project. colud any body help me.?? AttachmentPI demo.zip (176 Downloads) |
1/31/2008 12:18 PM | |
Joined: 8/25/2005 Last visit: 10/5/2024 Posts: 1162 Rating: (111) |
Hello Abdelaal, you didn't wrote about the CPU type and firmwareversion you are using. Have you checked that both CPU's got the same? Maybe an update of the firmware solve your problem. Within this foulder you will find a lot of new firmware versions. Hope this will help you Best regards Sabine |
5/21/2008 8:20 PM | |
Posts: 510 Rating: (117) |
What are the errors in the Diagnostic Buffer of the CPU with the faults? |
Follow us on