10/14/2016 1:49 PM | |
Joined: 11/14/2008 Last visit: 5/6/2024 Posts: 504 Rating: (22) |
17.5.1 "SIMATIC S7 Protocol Suite" Channel - Diagnostic Options Checking the Communication Processor Configuration Besides checking the access point, the communication processor can be tested with the "Set PG/PC Interface" application. The communication processor can be checked under SIMATIC NET in the same way Next manual explains how you can set up communication : SIMATIC WinCC V7.0 Getting started Regards, |
This contribution was helpful to1 thankful Users |
4/20/2017 4:33 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4766 Rating: (122) |
New question published by norimane is split to a separate thread with the subject How can i do communication between s7300 and wincc in real time. Best regards |
Follow us on