4/24/2017 8:57 PM | |
Posts: 200 Rating: (6) |
Hi i have a little sample of a small program that i am trying and wounder if there are some suggestions for the following. I1 and I2 are fault inputs from external devices. I1 will make the beacon/sounder pulse I2 will be steady what i need to do is from a push button that is on the panel mute the strobe and sounder until the faults are cleared. when the system restarts. Thanks Andrew AttachmentBeacon Mute.zip (199 Downloads) |
4/24/2017 9:22 PM | |
Joined: 12/18/2014 Last visit: 9/6/2024 Posts: 33709 Rating: (4186)
|
Maybe like this?
Attachmentbeacon_mute_V2.zip (238 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on