5/3/2017 7:33 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1051) |
hi Reyntjensmi, have a look to the following manual. SIMATIC S7-300 CPU 31xC and CPU 31x: Technical specifications in Chapter 8.7 you find a block diagram of the integrated digital I/Os: As you can see, the module needs a M that the LEDs can ligth up. Without any wiring on the modules the LEDs won´t work. hope this helps, regards, |
FCK WAR! |
|
This contribution was helpful to2 thankful Users |
5/3/2017 9:36 AM | |
Joined: 5/28/2008 Last visit: 6/7/2024 Posts: 4508 Rating: (837)
|
Hello, Just a small info to add, Please check that the Inputs / Outputs are inside the PII / PIQ of the CPU. The following link summarize the steps you have to follow (as instructed from my friends here) Hope this helps. |
Ayman Elotaify |
|
This contribution was helpful to2 thankful Users |
Follow us on