5/8/2017 12:45 PM | |
Joined: 3/2/2007 Last visit: 7/26/2024 Posts: 932 Rating: (5) |
we have Scout v4.2 engineering software installed on a virtual machine Vmware with windows Xp . when we try to go online on the Simotion , it takes several minutes ... what could be the cause . note that the used host laptop is very fast with solid state hard disk and windows 7 64 bits . Simotion D4xx v4.1 sp5 , Sinamics v2.5 , Bootloader v2.10 , PN v2.2 6AU1445-0AA00-0CA0 , SIMOTION DRIVE-BASED MULTIAXES BUNDLE D445 CONSISTING OF 1 UNIT EACH PROGRAMMABLE MOTION CONTROLLER D445 (6AU1445-0AA00-0AA0) + CF (6AU1400-2PA01-0AA0 -Z M44) WITH MULTIAXES PACKAGE LICENSE |
... thank you ... |
|
Follow us on