8/3/2007 2:26 AM | |
Posts: 33 Rating:
|
Thanks for your reply lkkezklf, Your idea is one of sollutions, but I hope that there is a more simple one. |
5/29/2008 1:26 PM | |
Joined: 2/22/2006 Last visit: 7/3/2024 Posts: 290 Rating:
|
Hi, The idea of Salma is pretty simple. Please put any of the objects in Siemens HMI Symbol Library. I would suggest you to use "Software digital point" from ASHRAE Controls & Equipment. Make SymbolAppearence = Hollw, Stretch = Yes.Put the object on top of your object. Next on Object Properties, Event page, Object Events, there is MouseMove event. Here you can bind some action (C or VBS) to do something when user place mouse pinter over the rectangle. One of the disadvantages is that the color of the rectangle (Software digital point) could not be changed, so you will have black howwol rectange arrownd the objects. If you want you can consider another idea. Place a button over your objects with Dynamic Filling = Yes, amd Fill Level = 0. I am 100% aggreed with the opinion of Ikkezelf - this thing are definetly not important!!! regards, Svetozar Yolov |
Follow us on