5/12/2017 7:00 AM | |
Posts: 2 Rating:
|
Good day all I am struggling to get WinCC 7.3 to function as OPC client with CoDeSys 3.5 OPC Server. Yet an other OPC client functions perfectly fine. Why?
Server Machine:
My current thoughts are around the security. I cannot get WinCC to generate a certificate when following the steps in the system manual, even when I've deleted them. No "Rejected" folder is ever created for certificates. After spending too many hours on this, I am at a loss. Any assistance would be welcome. ps. Results are the same when connecting to the CoDeSys OPC server installed locally on the Client machine (regarding OPC UA). The local OPC server however also communicates using OPC DA, and this works with WinCC. However, UaExpert works regardless. Any thoughts? Regards, Andrew AttachmentAttachment.zip (145 Downloads) |
Last edited by: Andrew_E at: 5/12/2017 7:02:29 AM |
|
Follow us on