5/13/2017 8:58 AM | |
Joined: 1/17/2017 Last visit: 9/25/2024 Posts: 5 Rating: (0) |
Hello. From when is max cycle time measured? From last restart of CPU? I have max cycle time over 120 but current cycle time is around 30. Even if I click update several times never jumps on 120. Mean that in history once was 120? ------------------------------------------------------------------------------------------ |
Last edited by: arozma at: 5/13/2017 9:11:16 AMLast edited by: arozma at: 5/13/2017 9:24:10 AMLast edited by: Min_Moderator at: 5/15/2017 2:57:08 PMNew subject after splitting |
|
5/16/2017 7:11 AM | |
Joined: 12/9/2010 Last visit: 10/8/2022 Posts: 623 Rating: (77) |
Hi arozma, The scan cycle time is not consistently same due to time OBs (OB3x), interrupt OBs or conditional jumps or calls within user program. No need to bother about max cycle time!!!!!!! |
If you like the comment, rate it (right top) or thank it (left bottom). |
|
Follow us on