5/20/2017 11:14 AM | |
Joined: 2/2/2015 Last visit: 9/26/2024 Posts: 124 Rating: (21) |
Hi Pandiani, You may need to change your picture width and height during configuration as the following: Let's say that the two screens with resolution 1280 x 1024 each so 1- Create a PDL with size 2560 x 1024 2- In this PDL create two PDL ( Picture window ) having the two view you need with pixels 1280 x 1024 each 3- The first PDL should take the coordination (0,0) and the second should start after finishing the first at (1024,0). you could find also some info about splitting screen in the following FAQ. Hope this helps Regards; Ahmed Kadry |
This contribution was helpful to1 thankful Users |
Follow us on