Industry Online Support
Technical Forum
6/2/2017 8:04 AM | |
Joined: 12/1/2012 Last visit: 7/30/2024 Posts: 128 Rating:
|
Dear Sir , Please find the attached file of System Architecture in Project . Description PC1 and PC2 is connected through NIC1 card for Redundancy . I am facing following problems. 1. When Both PC is in run time i am getting double entries for User Archive. User archive synchronization is active. So first question is why double entry is coming ? To avoid double entry of user archive i have done scripting like only master PC will execute and single entry will come . But During NIC1 Card network error comes and master PC gets off . Standby PC becomes master as per redundancy concept . 2. Second question Status of Master and Standby only depends on NIC1 communication means both PC mandatory require Connected through cable ? If Master PC-> truncated ... AttachmentSystem Architecture _Descrition of WinCC Redundancy.pdf (61 Downloads) |
Follow us on