Industry Online Support
Technical Forum
6/3/2008 4:07 AM | |
Posts: 510 Rating: (117) |
http://support.automation.siemens.com/WW/view/en/26283062 This link is an excellent example for what you are looking for. You have to modify the scripts to conform to your configuration. The SQL Database and the WinCC Flexible PC Runtime can both run on the same PC. Bill |
6/3/2008 6:07 PM | |
Posts: 510 Rating: (117) |
I used the WinCC V6.2 SQL Server 2005 SP1 and it ran on XP SP2. I have a colleague that did an application note for MS Access. I have attached the note for your reference. Bill AttachmentLog Data to ODBC Database AppNote.zip (485 Downloads) |
6/4/2008 12:05 AM | |
Posts: 58 Rating: (0) |
Thank you im going to check it |
Follow us on