6/12/2017 5:02 PM | |
Posts: 25 Rating: (0) |
Greetings. I have a CPU 317 - 2DP that keeps the SF led lighting and the BF2 flashing continbuosly. The PLC can't get to run mode; after a blackout when the energy turned on the PLC went to Stop mode automatically. The network it seems ok because all the nodes are OK in green. This was the diagnostic buffer that we was able to extract (file attached). Please help me finding the problem, I'm new working with PLC siemens so I have no experience reading the faults. Thanks. AttachmentDiagnosticBuffer050617.txt (61 Downloads) |
Follow us on