6/12/2017 12:54 PM | |
Joined: 4/28/2015 Last visit: 6/3/2024 Posts: 3345 Rating: (378)
|
For example you can use WinSCP to copy the folder. You can copy data from the Windows filesystem per Drag&Drop to the filesystem of the IOT2000. Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
6/12/2017 2:04 PM | |
Joined: 2/20/2014 Last visit: 6/11/2024 Posts: 396 Rating: (38) |
Hi, i have done as per your reply but i only have the SIMATIC IOT2000 Digital Input but not the user led
|
6/12/2017 2:12 PM | |
Joined: 2/20/2014 Last visit: 6/11/2024 Posts: 396 Rating: (38) |
Sorry, i had used a wrong path to select the files. The other path contained partial files. Now after using the correct path the other node is here.
|
6/14/2017 8:24 AM | |
Joined: 4/28/2015 Last visit: 6/28/2024 Posts: 578 Rating: (43) |
This is a useful contribution to the current image release! However, I think we should address this gap on the long run via the underlying abstraction library mraa. Two reasons for that:
Note that the need for polling on digital input changes is gone with the latest developer image from https://github.com/siemens/meta-iot2000. Contributions are always welcome, let us know so that we can synchronize the activities and avoid duplicate work. |
Follow us on