10/28/2014 1:15 PM | |
Posts: 15 Rating: (0) |
Hello I had to return the original backup program but the event that came up was as described above. I need lots of help
|
10/28/2014 1:35 PM | |
Joined: 8/27/2010 Last visit: 4/13/2024 Posts: 417 Rating: (37) |
In urgent cases is better to provide complete diagnostics buffer and your program for faster examination, as proposed byMarcjan |
This contribution was helpful to1 thankful Users |
10/28/2014 1:52 PM | |
Posts: 15 Rating: (0) |
Dear, Follow the diagnóstiscos as required. The only error that appears now is not the STOP. Only when I create some FC or DB generates the error: Stop Caused by priority class system Event: Current event initiaded OB1 start by end of OB1 (cycle free) OB number: Cycle program (OB1) Priority class: 1
AttachmentDiagnose - Bloco de notas.pdf (367 Downloads) |
10/28/2014 2:00 PM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1054) |
Dear Sabará, please see the following FAQ http://support.automation.siemens.com/WW/view/en/906270 when your programm is running in OB35, which time is set for this OB? Be sure that the time is enough. |
Last edited by: mopS04 at: 10/28/2014 2:03 PMFCK WAR! |
|
This contribution was helpful to1 thankful Users |
6/9/2017 4:10 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4767 Rating: (123) |
New question published by niksss is split to a separate thread with the subject Problem with CPU 314C-2DP for Redudancy. Best regards |
Follow us on