6/27/2017 3:35 PM | |
Joined: 9/27/2006 Last visit: 4/26/2024 Posts: 12257 Rating: (2665) |
Hello niksss; To complete the request for information from Duris, start by reading the chapter on "Communicating over a network" in the following manual; concentrate on the section discussing connections with the S7-300: Here are 3 FAQs explaining how you can connevt to a s7-300 through MPI, through Profibus-DP and through Ethernet, if your CPus have the correct interface modules: Communication between s7400 and s7-200 via em277 Once you have determined the type of network you will use to exchange between your S7-200 and your S7-300, come back to the forum if you need more information. Hope this helps, Daniel Chartier |
This contribution was helpful to2 thankful Users |
Follow us on