7/4/2017 7:13 AM | |
Joined: 5/12/2006 Last visit: 7/11/2024 Posts: 22308 Rating:
|
Hello, this is not possible because the IPC627D doesn't support the OS Win2000. You can only try it with a Support Request but i think there are no driver available, for this IPC was never Win2000 released. Regards Christoph |
7/4/2017 7:15 AM | |
Joined: 3/14/2008 Last visit: 7/11/2024 Posts: 2075 Rating:
|
Hi, I don't think this is possible, because I also can't find any drivers for it. Only for OS Windows 8.1 and Windows 10. Since it is a box PC, I don't think it works with VMware... VMware is not released for PCS7, but it can work in a normal PC. |
If I could help you, you can use the RATE button. Thank you. |
|
7/4/2017 11:08 AM | |
Joined: 10/26/2011 Last visit: 6/12/2024 Posts: 762 Rating:
|
Windows 2000 is released for the following PCS 7 versions:
With the compatibility tool, Industry Online Support provides a function, with which you can put together a compatible selection of software products or with which you can check the existing configuration for compatibility: |
Last edited by: Thunderstorm at: 8/9/2017 11:33:42 AMLast edited by: Thunderstorm at: 8/9/2017 11:34:17 AMSIMATIC PCS 7 - Overview |
|
Follow us on