6/22/2017 7:28 AM | |
Joined: 10/18/2012 Last visit: 12/15/2023 Posts: 225 Rating: (23) |
Hi Oly_Oliver, what I would do is - make a full backup image of the current system (i.e. with SIMATIC Image & Partition Creator) - figure out, if it is a hardware problem or software problem (try to boot linux os from usb) - (optional) re-install the operating system and required applications - (optional) replace defective hardware components It's really nothing detailed, but the required action depends heavily on the specific situation. If you need assistance, Siemens provides some technical support. See https://www.siemens.com/automation/support-request for details. |
This contribution was helpful to1 thankful Users |
7/6/2017 3:13 PM | |
Joined: 6/19/2017 Last visit: 8/5/2024 Posts: 8175 Rating: (169) |
New question published by Jamesbarnhart is split to a separate thread with the subject Computer is restarting again and again - Help!. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on