7/3/2017 9:14 AM | |
Posts: 12 Rating: (0) |
Hi all ! Could you show me detail about configuration of communication between S7-300 with Siemens relay protection or please send to me a example about it. Many thank! ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 7/3/2017 2:53:24 PMNew subject after splitting |
|
7/3/2017 3:20 PM | |
Joined: 9/27/2006 Last visit: 5/27/2024 Posts: 12257 Rating: (2668) |
Hello huyhung; We need a bit mor einformation to help you out properly: - which relay will you be using? - what software (DIGSI 4, DIGSI 5) ? - what communication interfce do you have installed on the relay? - what communciation link are you planning to use? As an example, let's say you have a 7SJ80, with a RS-485 (Profibus-DP) interface installed in the rear panel of the relay, and you are usoing DIGSI 4 to configure the relay. First, some discussions from previous threads on communications over Profibus-DP with these relays: SIPROTEC Profibus communication with 315-2dp SIPROTEC 7SJ80 profibus interface Next, links to the downloads you need to install and/or study; this will correspond to the threads shown earlier: SIPROTEC Compact 7SJ80/7SK80 Communication module PROFIBUS-DP Bus mapping SIPROTEC 4 Communication module PROFIBUS-DP Communication profile SIPROTEC Compact - 7SJ80 - Device Driver Please note that the division of Siemens that maintains this forum (Siemens Industry) is not the same that produces the Siprotec relays (Energy/ Digital Grid). To locatethe documents you need for the Siprotec 4 and Siprotec 5 relays you have to access and search their site: Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 7/3/2017 5:13:19 PM |
|
This contribution was helpful to1 thankful Users |
7/4/2017 4:03 AM | |
Posts: 12 Rating: (0) |
Hi dchartier, Many thanks for your help. It 's very useful to me - I'm using : Siprotec 7UT61. And software is DIGSI 5 - Communication interface which I have installed on the relay is RS-485 (Profibus - DP) - And I wanna link communication Profibus - DP between PLC S7- 300 CPU 315 -2DP and relay Siprotec 7UT61. So Do I need another module ( as CP - Communication Module ) to do it?
|
Last edited by: huyhung at: 7/4/2017 4:19:04 AM |
|
7/7/2017 1:53 PM | |
Joined: 9/27/2006 Last visit: 5/27/2024 Posts: 12257 Rating: (2668) |
Hello huyhung; I remember working with Digsi 4.x and having to install Step 7 on anoyher partition, it was impossible to install bith concurrently on the same OS. Digsi 5 can be installed alongside Step 7 v5.5, as you can read in the Product Information document: http://w3.siemens.com/smartgrid/global/en/products-systems-solutions/protection/engineering-evaluation-diagnostic-software/pages/digsi-5.aspx (open Manuals, Digsi 5) STEP7 V5.x The usage of DIGSI 5 V7.30 and the automation software STEP 7 V5.x on the same system is possible without restrictions. Hope this helps, Daniel Chartier |
Follow us on