7/8/2017 6:16 PM | |
Joined: 2/11/2015 Last visit: 8/30/2024 Posts: 462 Rating:
|
Hi, I've a S7-1500 and every modification (even if I change a contact) that I do, when I go to download it says that not enough memory to load. At this moment, I stop CPU, erase data and I could load the block/s. On online the CPU has 95% Memory Load and 10% rest of memories. There is any solution in order download?¿ ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 7/10/2017 9:53:02 AMNew subject after splitting |
|
7/10/2017 10:19 AM | |
Joined: 7/9/2015 Last visit: 8/30/2024 Posts: 3943 Rating:
|
Hi, you need a bigger SMC. Your loading memory is 95%. If you download changes, the program code exists for a little while twice. When Download is finished, new code will be copied to RAM and then the old code will be deleted... Also check the follwoing FAQ When downloading to the S7-1500 CPU, why is the message "There is insufficient memory on the memory card for this amount of data" displayed although there is still enough memory available?Regards, Towome |
|
|
Follow us on