Industry Online Support
Technical Forum
1/5/2011 10:03 AM | |
Posts: 50 Rating: (6)
|
Hello, I guess there is a mistake in the PAC4200 parameter settings. The SENTRON PAC4200 meter has two gateways: "serial gateway" and "modbus gateway" Look to the attached file, please. There you can find an example for a SENTRON PAC3100 device firmware update.The second example use ethernet Modbus TCP/IP connection via SENTRON PAC4200 serial gateway. The attached *.spl file is a SENTRON powerconfig V2.1 sheet. AttachmentExample_Description.zip (1041 Downloads) |
This contribution was helpful to2 thankful Users |
3/17/2011 9:04 AM | |
Posts: 9 Rating: (1) |
Thanks Rynite. You are right I change the configuration from ModbusGateway to Serial Gateway and its works. |
7/11/2017 2:11 PM | |
Posts: 1 Rating: (0) |
Many thanks for your help - sorted Cheers Simon |
Follow us on