7/16/2017 10:32 AM | |
Joined: 1/3/2013 Last visit: 9/12/2024 Posts: 40 Rating: (3) |
Dear friends, I would like to know you opinion above the following. In an application we need to integrate two flow-meters generating pulses at 5ms. I'm thinking of using 2 counting channels of S7-314C. Doing a quick forum search and reading the manuals I found that this PLC might do the job, even it is more likely to be used for positioning application. Did I had a correct understanding? I'm using TIA Portal V13 SP1 Upd9. In HW configuration of Counting channels there is something that doesn't looks right or I might have a different understanding. As in CPU 31xC: Technological functions What happens with the assigned DI and DO if not all of counter functionalities are to be used? Let's say that I don't need a signal on the DO of the counter channel. Can I use this DO for other purposes since I'm pretty low on DOs for the overall application? Best regards! Mircea. AttachmentCounting-Channel-Hw.pdf (53 Downloads) |
Follow us on