7/14/2017 6:41 AM | |
Joined: 7/8/2014 Last visit: 7/2/2022 Posts: 14 Rating:
|
Dear Mr. Kaulquappe Please help me on choosing module and license for the configuration in attached picture. Required: Modbus TCP redundancy In my system: - Client side: Hot/Standby CPU system (not Siemens product), the master and slave CPU will swap IP address when master switch over. Each CPU using two Ethernet channels (with different subnet .1, .2). - Server side: I am going to use two CP343-1 for Modbus redundancy, but each CP will connect to one HUB. Data received from client will be transfer to Siemens IO module to control actuators. My questions: 1. Can I use two CP for redundancy connect to Master (CPUA or B) via two different HUBs, and with different subnet (with the license: 6AV6676-6MB30-3AX0) 2. If the answer is NO: - Will I have to write logic on Siemens CPU myseft to select which channel (P or Q, CP1 or CP2) to communicate? - And in this case, the license will be 2XV9450-1MB00, that's right? Thank you! Tan ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 7/14/2017 1:14:20 PMNew subject after splitting |
|
7/17/2017 7:54 AM | |
Joined: 7/8/2014 Last visit: 7/2/2022 Posts: 14 Rating:
|
Thank you Mr. Kaulquappe for your helpful answer! Best Regards, Tan |
Follow us on