5/6/2008 11:01 PM | |
Posts: 2661 Rating: (279) |
mith: Which blocks are you not able to convert to S7? Normally standard blocks (like communication functions etc.) are locked (protected). These blocks cannot be converted form S5 to S7. They have to be manually replaced by equivalent S7 blocks. Look at the following FAQ for further help. Considerations for the conversion of S5 programs to S7: http://support.automation.siemens.com/WW/view/en/14529143 Regards |
8/11/2010 5:20 PM | |
Posts: 1 Rating: (0) |
can you explain how do it |
8/11/2010 5:39 PM | |
Joined: 9/27/2006 Last visit: 6/19/2024 Posts: 12260 Rating: (2671) |
Hello shervin; Have a look at a recent discussion that was held on another forum, it shows how to use the deassembled S5 code to modify the BE settings: http://www.plctalk.net/qanda/showthread.php?t=57199&highlight=s5 Hope this helps, Daniel Chartier |
8/1/2017 2:36 PM | |
Joined: 6/19/2017 Last visit: 6/12/2024 Posts: 8140 Rating: (165) |
New question published by Yesha925 is split to a separate thread with the subject How to open the protected blocks? . Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on