8/2/2017 4:10 AM | |
Joined: 4/28/2015 Last visit: 6/3/2024 Posts: 112 Rating: (3) |
Dear All, I am using a s7-200 plc and an OP. I have all the alrams in the Protool alarm list and there are numbers noted on the sides. I have also noted the alarm messages in the VM 60 area. and Event messages in the VM 50 area. How do I understand the which bit triggers a particular alarm for example:" Communicationerror frequencey contoller -A02" Please help Thanks AttachmentDesktop.zip (237 Downloads) |
Thanks |
|
Follow us on