8/3/2017 2:27 AM | |
Posts: 31 Rating: (0) |
Hi there, I have the following NPN Sensor which is 2 wire. Would a standard sourcing 6ES7131-4BD51-0AA0 module work with this type of sensor or will i need resistors to simulate a load? From the drawing, i would wire Brown (+V) to the input of the sourcing module DI, and blue to the M. Hope to hear from someone, AmazingTrans |
8/3/2017 10:15 AM | |
Joined: 8/31/2005 Last visit: 4/26/2024 Posts: 2197 Rating: (326)
|
I think: yes, it will work. |
|
|
Follow us on