8/1/2017 1:43 PM | |
Posts: 10 Rating: (0) |
Hi All, I hope that someone can help me or direct me in the right direction. I would like to send data from my IOT2040 to a LOGO!8. How would the setup on both the IOT/ Node red and LOGO! be done. I am able to send data from the LOGO! to the IOT2040 but it is the communication in the opposite direction that I am having a problem with. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 8/1/2017 2:59:27 PMNew subject after splitting |
|
8/1/2017 2:06 PM | |
Posts: 215 Rating: (6) |
How are you communicating? Are you using the s7 nodes? Can you show us your configuration? (Mark the nodes and export them) |
8/2/2017 9:58 AM | |
Posts: 10 Rating: (0) |
Yes I am using S7 communication on the Logo! and Node red See the attached screenshots AttachmentIOT nodes.zip (791 Downloads) |
8/2/2017 10:12 AM | |
Posts: 215 Rating: (6) |
It seems like you are trying to write on an input of the logo. I'm not sure that's permitted. Have you tried writing on the memory or data blocks? |
Follow us on