3/20/2017 10:26 AM | |
Joined: 9/9/2015 Last visit: 11/12/2024 Posts: 728 Rating: (280) |
Is this solved? May I know how to create a button to acknowledge the Optipno? I can make a button to set the optipno to "0", but it would not generate any operator messages in the operational alarm logging. Can anyone help on this? |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
8/5/2017 5:32 AM | |
Joined: 9/9/2015 Last visit: 11/12/2024 Posts: 728 Rating: (280) |
Here i consolidate with few ways of generating Operator message and show it in Alarm Control, or by using Optipno, Digital input and Analog input. If it is helpful, you may rate my post. If you have any better ideas, feel free to comment. Thanks! AttachmentOperator Message Testing.zip (156 Downloads) |
Last edited by: JazTai at: 8/5/2017 5:34:33 AMPlease give me 5 stars Rating if my post is helpful for you. :) |
|
This contribution was helpful to2 thankful Users |
Follow us on