8/21/2017 4:58 PM | |
Joined: 10/3/2016 Last visit: 5/7/2024 Posts: 38 Rating: (0) |
Dead Sirs, I am trying to establish a Profinet communication between S7-1215C DC/DC/DC and an S110 CU305 PN servo drive: - I added S110 GSD files in the TIA portal - I added a telegram in TIA portal - I set drives by STARTER: model, power module type, IPs, same telegram, some base settings - I set IP of each device - hardware connection between s7-1200 and S110 does not work. At my hardware configurations I have errors in lower level components which are not clear enough to explain. I have added some photos on the attachment. I am so confused, feel free to ask for any TIA or STARTER photos. AttachmentS110.zip (124 Downloads) |
Last edited by: The Troodon at: 8/21/2017 5:03:18 PM |
|
Follow us on