8/22/2017 7:47 PM | |
Joined: 10/2/2014 Last visit: 3/26/2019 Posts: 2 Rating:
|
Hi Support, I have a IoT2040 and have followed all setup and installation guides. I can connect through PuTTy and WinSCP to the device, Node Red also starts and is accessible. I can ping any IP I choose. Internet and local network connections are active and remain active. As soon as I connect the IoT2040 to a hub, so I can connect to the IoT with other devices, I am not able to connect to the device anymore. In essence, direct connection to the IoT works but any connection via a hub or router does not connect. Any suggestions? Regards, Harald, ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 8/23/2017 7:37:22 AMNew subject after splitting |
|
Follow us on