8/28/2017 9:35 AM | |
Joined: 9/27/2007 Last visit: 12/18/2020 Posts: 993 Rating: (102)
|
Dear Harpreet, Flash Storage: \flash\.... SD Card: \Storage Card SD\.... With best regards cumulus |
Last edited by: cumulus at: 8/28/2017 9:35:22 AMLearn more about visualization - visit the HMI courses of Siemens AG! |
|
8/28/2017 10:41 AM | |
Posts: 8 Rating: (0) |
Dear Cumulus, I used the path in script but problem is whenever I simulate script on my local workstation or PC it runs fie but on HMI it doesn't make or saves any file ??Any clues.. attaching my script file also..
AttachmentTP700 script.txt (188 Downloads) |
8/30/2017 3:53 PM | |
Posts: 648 Rating: (95) |
Dear harpreet, you use vbs methods/functions which are not avaible for Windows CE. Like "CreateTextFile" or "GeFile". So this script cannot work. The OS on the Panels is Windows CE not Windows 7/10. Look at the programming reference for WinCC Advanced, chapter 1.3 (page 106) https://support.industry.siemens.com/cs/ww/en/view/109747176 Also you can find a inspiration of data handling and scripting in the toolbox for HMI projects. https://support.industry.siemens.com/cs/ww/en/view/106226404 With best regards |
Follow us on