9/1/2017 7:24 AM | |
Joined: 7/19/2017 Last visit: 9/29/2024 Posts: 64 Rating: (0) |
Hi, I am trying use the wifi module that insert to the mpice port of iot2040 to connect the ethernet. But i found it can not be worked, and i did not see the wlan0 in the configure network interfaces, just eth0 and eth1, and all of them i already set to the dhcp. What did i do to connect the ethernet through the wifi module ? Best regards
------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 9/4/2017 2:33:13 PMNew subject after splitting |
|
9/1/2017 7:59 AM | |
Joined: 4/28/2015 Last visit: 9/9/2024 Posts: 3345 Rating: (379)
|
Hi, I think with Ethernet you are thinking about the Internet, aren't you? Which mPCIe card are you using? It may be that the drivers for it are missing. You can have a look at this post. There are some tested cards listed. Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
9/1/2017 9:57 AM | |
Joined: 7/19/2017 Last visit: 9/29/2024 Posts: 64 Rating: (0) |
Hi felixxx, I want to know how to copy the driver file that download from forum in windows to the /lib/firmware in linux ? Forgive me did not familiar with the linux operation. best regards
|
9/1/2017 10:51 AM | |
Joined: 4/28/2015 Last visit: 9/9/2024 Posts: 3345 Rating: (379)
|
You can use e.g WinSCP to transfer data from Windows side to the IOT2000. Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
This contribution was helpful to1 thankful Users |
9/1/2017 11:02 AM | |
Joined: 7/19/2017 Last visit: 9/29/2024 Posts: 64 Rating: (0) |
Thank you so much, I will try for that .
|
9/4/2017 8:36 AM | |
Joined: 7/19/2017 Last visit: 9/29/2024 Posts: 64 Rating: (0) |
Hi bergmanu, Yes, i want to use the wifi card connect to the internet. The mPCIe card that I am using is SIM7100C, yes it need to install drivers, but i do not know how to install it . According to the instruction i can not found the "/driver/usb/serial/option.c" path in the v2.1.3 image . So have you used it before ? best regards
|
Follow us on