9/5/2017 5:22 PM | |
Posts: 5 Rating: (0) |
Hello, everyone, i want to ask a question, that s7 1516 supports modbus protocol and how can man enable this modbus in cpu via Tiaportal V14? Regards Fei Yin |
9/5/2017 5:45 PM | |
Joined: 9/27/2006 Last visit: 10/14/2024 Posts: 12287 Rating: (2685) |
Hello Fei Yin; The S7-1500 CPUs all support Modbus, both Modbus RTU (master or slave) and Modbus TCP (client or server): Modbus RTU: Modbus TCP: How do you program and parameterize Modbus/TCP communication between S7-1500 CPUs and S7-1200 CPUs? These functions are all available under TIA Portal v14. Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 9/5/2017 5:45:33 PM |
|
Follow us on