9/7/2017 10:09 AM | |
Joined: 4/28/2015 Last visit: 6/3/2024 Posts: 3345 Rating: (379)
|
Hi, why do you want to update the npm mraa? We do have installed the version 1.5.1 installed in our example image, the lib itself and the npm version. In my opinion there is no need to update the npm version. A possible reason that your update is not working (nodes are not present any more) is that the current npm mraa version (1.7.0) requires a newer node.js version. There is V6.9.2 installed in the example image. We had the same problem with the OPC UA nodes. If there is an incompatibility the node are not in the pallet. Best regards! ------------------------------------------------------------------------------------------------------ EDIT: please try these nodes: https://support.industry.siemens.com/tf/ww/en/posts/specific-nodes-for-iot2000/176929/?page=0&pageSize=10 ----------------------------------------------------------------------------------------------------- |
Last edited by: bergmanu at: 9/7/2017 12:58:44 PMNot working for IOT2050 support anymore from March 1st, 2024. |
|
Follow us on