7/27/2017 2:23 PM | |
Posts: 7 Rating: (0) |
hy everyone, i can connect with IM151-3BA23-0AB0, in profinet i checked all the conections, i name it i put the correct IP, when i do browse does not see anything.... ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 7/28/2017 12:14:59 PMNew subject after splitting |
|
9/7/2017 9:44 AM | |
Joined: 5/12/2006 Last visit: 5/2/2024 Posts: 22243 Rating: (2981) |
and to which interface is the IM connected ? And is the PC on the same interface? |
9/19/2017 10:08 AM | |
Posts: 7 Rating: (0) |
hi, i found the right answer in a old post : Hi Everybody, SOLUTION: normally DLC is installed automatically. Thanks all. |
Follow us on