9/22/2017 5:07 PM | |
Posts: 42 Rating:
|
Sir mpso4 and sier daniel carter i have attached the screenshot you were asking for if you want any more plz ask. Sir i have also uploaded the sideways pic of module plz sir after reading tell me i am giving 24V dc at pin 10 and 0v dc at pin 20 & also 24 v dc at pin 1 & pin 11 is that enough to turn on leds because the plate reads 30v dc/250v ac & 125 v ac moreover the plate of card reads sm 322 d0 16*rel.120V AC
AttachmentSios.zip (291 Downloads) |
Last edited by: Programming Lover at: 9/22/2017 9:32:02 PMLast edited by: Programming Lover at: 9/22/2017 9:36:19 PMLast edited by: Programming Lover at: 9/22/2017 9:38:11 PM |
|
Follow us on