10/25/2017 12:06 PM | |
Joined: 9/2/2013 Last visit: 11/6/2020 Posts: 48 Rating:
|
There is a helpfully program named ser2tcp. set2tcp is a bridge between local serial ports and tcp ports. How build it: Download source from https://sourceforge.net/projects/ser2net/ to a folder on IOT2000. Change to this folder with cd <folder> tar xvzf ser2net-3.5-rc3.tar.gz cd ser2net-3.5-rc3 ./configure make make install You can call ser2net with this parameter: ser2net -c <tcpport>:<timeout>:<protocol>:<serialdevice>:<baudrate> For example to share X30: ser2net -c 2040:raw:60/dev/ttyS2:19200 For multiple ports you can add a file /etc/ser2net.conf For detail: https://linux.die.net/man/8/ser2net On Windows you can install a serial port with tcp access: https://www.hw-group.com//products/hw_vsp/index_en.html (Single port is free to download, please see License – Distribution and Usage Conditions) |
Last edited by: Ocean_ at: 10/25/2017 12:08:56 PMLast edited by: Ocean_ at: 10/25/2017 12:13:55 PM |
|
This contribution was helpful to
2 thankful Users |
Follow us on