11/2/2017 1:50 PM | |
Joined: 1/4/2007 Last visit: 5/2/2024 Posts: 1116 Rating: (174)
|
Hello alexlub, That’s a strange behaviour! The weight values: - "DB_SIWA_U".i_GROSS_WEIGT_CH1//DB9.DBW12 -"DB_SIWA_U".i_GROSS_WEIGT_CH2//DB9.DBW20 are also in the Periphery Input Area of the PLC! The weight values can be seen at the Periphery Input address (see also the ttached file): - Channel 1: PIW [start address of the Siwarex U module in the HW-Config + 2] - Channel 2: PIW [start address of the Siwarex U module in the HW-Config + 10] Can you see in the Periphery Input address the weight values? Best regards Siwarexi AttachmentIO_Communication_SIWAREX_U_en.pdf (92 Downloads) |
Follow us on