10/27/2017 5:29 AM | |
Posts: 40 Rating:
|
Hi, [snip] I now encounter another problem. When I run the application via Eclipse as a "Remote Application". The application program can be downloaded to IOT2040, and can be runned via putty. However, every time I run the application as a "Remote Application" via Eclipse. The followed "Permission denied" error will be showed:(see the attached figure). No matter where I put the application (e.g. "/home" or "/home/root", etc.) on the IOT2040. When Eclipse connects to the Linux on IOT2040, do I need to set the user persimmion for Eclipse? ------------------------------------------------------------------------------------------ |
Last edited by: eric00058 at: 10/27/2017 6:22:02 AMLast edited by: Jen_Moderator at: 10/27/2017 8:01:46 AMNew subject after splitting Last edited by: Jen_Moderator at: 10/27/2017 8:03:46 AM |
|
11/1/2017 7:51 PM | |
Joined: 6/19/2017 Last visit: 6/28/2024 Posts: 8176 Rating:
|
New question published by eric00058 is split to a separate thread with the subject After I build the project, the 'HelloWorld' binaries file in the "IOT2000 Release" folder disappears. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on