5/6/2015 1:12 PM | |
Joined: 2/13/2013 Last visit: 4/19/2024 Posts: 2 Rating: (0) |
Meet a problem with first download of new CPU. There is no such (8.1) firmware version in HW config to configure HW station properly. I foud a HUP Hardware Upgrade Package "HUP CPU410-5H" Available for Download but it is not compatible with our PCS 7 8.0 SP2, only supports SP1. Does any bodye know the proper solution to work with that HW from SP2 PCS?
|
5/6/2015 1:57 PM | |
Posts: 567 Rating: (106) |
Hi,
have look at the application example "Process automation with the SIMATIC PCS 7 CPU 410-5H controller" Link: https://support.industry.siemens.com/cs/de/en/view/96839331 The HUP you want to install is in my opinion part of PCS 7 V8.0 SP2 and you only have to install it if you have PCS 7 V8.0 SP1. You can find the information about the first download of CPU 410-5H in chapter 2. |
5/6/2015 2:01 PM | |
Posts: 46 Rating: (3) |
Hi, please have a look at the released modules for PCS 7. Here you see that PCS 7 V8.0 SP2 only supports CPU 410 with FW V8.0.x (chapter 17.13)
To support FW V8.1.x you would have to upgrade PCS 7 to V8.1 (see chapter 17.14) regards |
Follow us on