6/23/2014 9:50 PM | |
Posts: 5225 Rating:
|
Hi Adrian, You have now.. B701 = 1 B702 = 12 --- right? By now you should have the manual from.. LINK Please go to page 156, and look for "ON reverse / OFF1". w |
8/9/2017 10:25 PM | |
Joined: 8/9/2016 Last visit: 7/5/2024 Posts: 70 Rating:
|
Definitely. Unfortunately i come across this problem 3 years later. |
8/29/2017 11:24 AM | |
Joined: 3/31/2015 Last visit: 1/26/2024 Posts: 175 Rating:
|
Because there is no minimum voltage. It'll pass anything up to max values. |
9/21/2017 5:11 PM | |
Joined: 9/1/2015 Last visit: 4/11/2024 Posts: 13 Rating:
|
Official Siemens answer is 3-35V DC. I've tested it with 12V DC and it works fine!! Hope it helps! Regards! Chucky! |
11/13/2017 7:12 AM | |
Posts: 1 Rating:
|
Why do I attach 24V to DO1, DO2 to the relay and then to 0V when the transistor also leads? What if I want the transistor to stop? |
Follow us on